Cancel
Showing results for 
Search instead for 
Did you mean: 

How to change the position of a loactions inside a seam?

Experimenter
Experimenter
Hello,
 
is there a way to change position of seam loactions inside a seam?
I know the command "Reverse Operation" is doing.
But 'MoveChildAfter()' method of a TxRoboticSeamOperation does not work / is not allowed (CanMoveChildAfter is false).
 
Best regards
3 REPLIES 3

Re: How to change the position of a loactions inside a seam?

Siemens Legend Siemens Legend
Siemens Legend

Hi,

 

The order in a seam operation represents the projected curve, so it is a constant.

 "Reverse Operation" command reverses the complete seam operation, so it still represents the projected curve – just from the other direction.

 

Regards,

Moshe

 

Re: How to change the position of a loactions inside a seam?

Experimenter
Experimenter

Sorry, i forgot my question.

 

Ok, but you can pick single seam locations of a seam (for example the secound and the fifth). "Reverse Operation" will only reverse the selected and the between locations.

A seam with locations s1, s2, s3, s4, s5, s6, s7 will be reversed to s1, s5, s4, s3, s2, s6, s7 if you pick s2 and s5 before calling "Reverse Operation".

 

Using several calls of "Reverse Operation" i can do a Move, but i am looking for a better solution.

Re: How to change the position of a loactions inside a seam?

Siemens Legend Siemens Legend
Siemens Legend

Hi,

Reordering of a seam operation is blocked since the seam locations correspond to the seam mfg.

What is the use case needed for reordering the seam operation?