Cancel
Showing results for 
Search instead for 
Did you mean: 

How to create a .cojt with TuneData.xml from the API

Siemens Phenom Siemens Phenom
Siemens Phenom

Starting from Tecnomatix V13.0.2, Tecnomatix .NET API provides new methods to create a TuneData.xml under a .cojt folder.

Here is an example that creates a new component with 3D, saves it to a valid .cojt and then imports it in the study.

 

            //1. Create a local component
            TxLocalComponentCreationData creationData = new TxLocalComponentCreationData("comp1", new TxTransformation());
            TxComponent comp1 = TxApplication.ActiveDocument.PhysicalRoot.CreateLocalComponent(creationData);

            //2. Add geometry
            TxBoxCreationData boxData = new TxBoxCreationData("box1", new TxTransformation(), new TxVector(500, 500, 500));
            comp1.CreateSolidBox(boxData);
            
            //3. Save it to .cojt
            string compFileName = "comp1.cojt";
            TxLocalStorage localStorage = comp1.StorageObject as TxLocalStorage;
            localStorage.SaveToLibrary(new TxLibraryData(TxApplication.SystemRootDirectory, compFileName));
            comp1.Delete();

            //4. Create prototype data file
            string path = TxApplication.SystemRootDirectoryNormalized + compFileName; 
            
            TxTunePmDocumentManager pmDocManager = new TxTunePmDocumentManager();
            TxTunePmDocumentPrototypeData data = pmDocManager.CreatePrototypeData("PmToolPrototype");
            pmDocManager.SavePrototypeDataToDocument(path, data);
              
            //5. Import the new component
            TxInsertComponentCreationData insertData = new TxInsertComponentCreationData("comp1", path);
            ITxComponent comp = TxApplication.ActiveDocument.PhysicalRoot.InsertComponent(insertData);
comp.SetModelingScope();
comp.EndModeling(path);

 

16 REPLIES

Re: How to create a .cojt with TuneData.xml from the API

Experimenter
Experimenter

Hello,

what is the ressource for

TxTunePmDocumentManager and TxTunePmDocumentPrototypeData

I don't find any information about that on the .net help.

 

Regards

Re: How to create a .cojt with TuneData.xml from the API

Siemens Phenom Siemens Phenom
Siemens Phenom

They are both from Tecnomatix.Engineering.dll.

The namespace of TxTunePmDocumentManager is Tecnomatix.Engineering.Utilities and the namespace of TxTunePmDocumentPrototypeData is Tecnomatix.Engineering.DataTypes.

These classes are avalable as of Tecnomatix V13.0.2

Re: How to create a .cojt with TuneData.xml from the API

Experimenter
Experimenter

So I just need to update,

thank you.

Re: How to create a .cojt with TuneData.xml from the API

Creator
Creator

Is it possible to dave a compound part using the method? We need to create compound parts or compound resources from individual JTs. Do you happen to have a sample code for that? Any caveats? 

Thanks

Re: How to create a .cojt with TuneData.xml from the API

Siemens Phenom Siemens Phenom
Siemens Phenom
Do you mean to create an End Item? Can you elaborate?

Re: How to create a .cojt with TuneData.xml from the API

Creator
Creator

We have a manual procedure for creation of equipment prototypes (for example dressed robots, complex fixtures, etc.).  

 

We need to automate the procedure. Parts to assembly the equipment prototypes are either .cojt or jt files. At this point it is mostly JT files.

 

 

Re: How to create a .cojt with TuneData.xml from the API

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

To create an equipment use that code:

//1. Create the equipment
TxPhysicalRoot root = TxApplication.ActiveDocument.PhysicalRoot;
TxLocalComponentCreationData epData = new TxLocalComponentCreationData("equipment1");
TxComponent eq = root.CreateEquipment(epData);

//2. Copy/Paste components under the equipment - components can be created as described in the example or if they are .cojt, you need to only insert them

//3. If needed create kinematics for the equipment using the ITxKinematicsModellable interface that is implemented by TxComponent

//4. End modeling the equipment
eq.EndModeling(eqPath);


Highlighted

Re: How to create a .cojt with TuneData.xml from the API

Creator
Creator

We are still using version 12.1 and:

TxComponent eq = root.CreateEquipment(epData); -- no such method
eq.EndModeling(eqPath); -- no such method


Any suggestions? 

 

 

 

Re: How to create a .cojt with TuneData.xml from the API

Legend
Legend

Hi,

 

the minimum version is 12.1.1

 

Look in the .Net helpfile:

The following items are new in version 12.1.1:

Modeling

The ability to set a selected component as modeling scope was added to ITxComponent .
The ability to end modeling and store a modeled object was added to ITxComponent .
The ability to create equipment was added to TxPhysicalRoot and TxComponent .