Cancel
Showing results for 
Search instead for 
Did you mean: 

How to pick vector coordinates

Pioneer
Pioneer
Which Picklevel is used for getting vector coordinates? I want to get x,y and z points when I click on graphics viewer
1 REPLY 1

Re: How to pick vector coordinates

Legend
Legend

Hi!

 

Pick level just specify which object will be selected if you click on entity in the graphic viewer: the entity or the component containing clicked entity.

"I want to get x,y and z points when I click on graphics viewer."

There is a problem, that you need an additional information in order to convert two coordinates of the click position inside graphic viewer to three coordinate of the 3D vector. Such information can be: constant value of one coordinate, any surface e.g. surface of the solid, or other 3D geometry.

 

Witalij.