Cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a way to implement "Geometric Gun Search" via .net API

Valued Contributor
Valued Contributor

PS provides a "Geometric Gun Search" command, Is there a way to implement this functionality via .Net API.

 

Thanks in advance fory any reply.

3 REPLIES 3
Highlighted

Re: Is there a way to implement "Geometric Gun Search" via .net API

Phenom
Phenom

Hello @kx

 

I'm pretty sure you can develop a customized version of GGS on your own. Actually this is something I was planning to do with some specific modifications to the application to then meet with my specific needs. 

 

Why do you want to implement it?

 

Regards,

Re: Is there a way to implement "Geometric Gun Search" via .net API

Valued Contributor
Valued Contributor

Hi @FredCastro

In PD, I am trying to assign a weld point from MFG library to a weld operation in a station process. The condition is that at least one gun in this station is able to reach the weld point. Since there are a lot of station processes in my project, It will take a lot of time to switch to PS using "Geometric Gun Search" to check if a weld point is reachable. This is why I want to implement it by API.

 

Is there an example of customizing GGS?

 

Regards,

 

 

Re: Is there a way to implement "Geometric Gun Search" via .net API

Phenom
Phenom

Hello @kx

 

I understood your issue! I also have the same problem with "Clone Collection" command, which I can only run in PD, not in PS. Unfortunately currently I don't have any implementation for GGS.

 

Regards!