Cancel
Showing results for 
Search instead for 
Did you mean: 

Process simulation 13.0.1- Mouse configuration

Pioneer
Pioneer

In PS, Right index finger is used for all the options like Pan, Zoom, rotate.

 

Since we are heavily using these options, it causes more stress to right index finger joints.

 

I checked customize mouse configuration but there is no option to avoid use of right index finger.

 

If we have an option to define shortcut key as shown below it will be very useful,

 

Pan        -> entire mouse + any one user defined key (e.g. - mouse + 1)

Zoom    -> entire mouse + any one user defined key (e.g. - mouse + 2)

Rotate  -> entire mouse + any one user defined key (e.g. - mouse + 3)

 

By using above shortcut,

We could achieve any movement just by pressing a key using left hand finger and moving entire mouse using right hand. 

 

Previously i was using tool called space vision which has similar shortcut keys like above example.

 

Is there any option to configure mouse as explained above?

or siemens could include such options in next release..

5 REPLIES

Re: Process simulation 13.0.1- Mouse configuration

Experimenter
Experimenter

There is some suggestions for you.

In the Tecnomatix 13, you can customize some operation such as mouse, ribbon, keyboard and so on. In the option named "customize the mouse", you can change these shortcut keys as you want to. I have already got used to CATIA's shortcut keys, so I modify them as the same as CATIA's.

My English is poor, so please ignore these grammer mistakes.

Betreff: Process simulation 13.0.1- Mouse configuration

Legend
Legend

I am not sure if I understand you correctly, but try to change mouse configuration to "Legacy".

Zoom -> Middle mouse button,

Pan -> Right mouse button

Rotate -> Middle and right mouse button

 

 

Betreff: Process simulation 13.0.1- Mouse configuration

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

Mouse configuration supports also Custom Configuration where you can define your own rules.

Right Click at the Ribbon Bar -> Customize the Ribbon... -> Customize Mouse

Then in Choose Mouse Configuration select Custom. The input fields will become enabled, then you can configure them.

 

Best Regards,

DianaG

 

Re: Process simulation 13.0.1- Mouse configuration

Pioneer
Pioneer
My intention is to avoid using index finger for Zoom, Pan & Rotate options.
But there is no option in current mouse configuration Smiley Sad

Betreff: Process simulation 13.0.1- Mouse configuration

Pioneer
Pioneer
My intention is to avoid using index finger for Zoom, Pan & Rotate options.
But there is no option in current mouse configuration Smiley Sad