Cancel
Showing results for 
Search instead for 
Did you mean: 

Sweep solids with more than 2 profiles

Experimenter
Experimenter

Hello,

 

we use the CreateSolidBySweep method to create solids via profiles.

If we create the TxSolidSweepCreationData.TxProfile[] with 2 polyline profiles everything works. But with more than 2 it doesn't. We get a TxUnknownErrorException with the message "Error in the application."

Can this method handle more than 2 profiles in the CreationData somehow or do we have to to call the method in a loop when we have more than 2 profiles?

 

Regards

Bjoern

1 REPLY 1

Re: Sweep solids with more than 2 profiles

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

Can you send us the code that fails, so we will investigate it. The function is supposed to work with several profiles, but there are cases with polylines that fail.

 

Best Regards,

DianaG