Cancel
Showing results for 
Search instead for 
Did you mean: 

Switch signal on that is connected to a logic block

Valued Contributor
Valued Contributor

Hi

 

How do I switch on a signal that is connected to a logic block. If I dont connect it then it can be done through the TxPlcInputSignal.value but when it is connected to a logic block the LB switches it according to its logic. So I what in this case like the force in the the panel viewer to overwrite the LB and keep the signal on.

 

Thanks

1 REPLY 1

Re: Switch signal on that is connected to a logic block

Siemens Phenom Siemens Phenom
Siemens Phenom