Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

TxLogWriter questions

Legend
Legend

Hello!

In one of my commands I use log4net with a memory appender.

Now I saw that the API has a TxLogWriter class and in the installation directory there is a log4net.dll.

Is TxLogWriter a wrapper of log4net?

If so, can I also use the TxLogWriter class with a memory appender? In the helpfile I can only read that it writes to the standard logfile. Where is the standard logfile?

 

2 REPLIES

Re: TxLogWriter questions

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

TxLogWriter writes in the application log file that can be activated from Tecnomatix Doctor. It is not a wrapper of log4net.

Re: TxLogWriter questions

Legend
Legend

Hello DianaG,

 

thank you for your answer. Then I will have to look for another solution.