Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

creation of Kinematic creation data

Siemens Legend Siemens Legend
Siemens Legend

Question:

.       Is there a class for the creation of Kinematic creation data?  i.e I would like to automate the process of creating kinematic but I can only find function and methods to change existing kinematic and nothing to make from scratch.

 

Answer:

 

  1. There is interface ITxKinematicsModellable that is implemented by all model objects that support kinematics (even not only devices, also objects that does not have kinematics yet).

Use that interface to:

  1. Get all TxJoint(s) and TxKinematicLink(s)
  2. Check if the model object supports kinematics and if it is open for modeling
  3. Couple TxJoints of different devices
  4. Create new TxJoint(s) and TxKinematicLink(s)
  5. Note: Kinematics is automatically compiled when creation is done and exception is thrown if compilation fails.
2 REPLIES 2

Re: creation of Kinematic creation data

Experimenter
Experimenter

Where can I find the ITxKinematicsModellable? I didn't found it at the Technomatix.NET.chm file and in Visualstudio implementing Tecnomatix.Engineering, Tecnomatix.Engineering.Ui

I try to get the velocitys of the Operations (e.g. viaLocationOperation)

Re: creation of Kinematic creation data

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Duren,

 

For the velocity check this article.

For ITxKinematicsModellable, it is implemented by every TxComponent, TxDevice, TxGun, etc.

Which version of Tecnomatix do you use?

 

Best Regards,

DianaG