Cancel
Showing results for 
Search instead for 
Did you mean: 

how to "Import eBop from File" with .NET ?

Pioneer
Pioneer

HI experts:

    I want to use TECNOMATIX.NET to implement the following functions:

    File-------Import---------Import eBOP from File 

  That is to use the program to import XML file .

   I wonder if there are any good ways.

    

3 REPLIES 3

Re: how to "Import eBop from File" with .NET ?

Pioneer
Pioneer

i find "LoadXml" method in Tecnomatix.NET chm, this method description is "Fills the TxSelectionFieldsDictionary with the data from the specified XML string." .but i don't understand what is "Selection Fields",and if this method can help me.

Please advise experts。

Re: how to "Import eBop from File" with .NET ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Dongyang,

 

The API does not expose a method to import eBop.

The method "LoadXML" that you found belongs to TxSelectionFieldsDictionary class. That class is used in the TxFieldsSelectionForm dialog which is a dialog where user can select from list of customized eMServer fields, it does not import an xml as Import eBop command.PropertiesCustomization.png

 

Best Regards,

DianaG

Re: how to "Import eBop from File" with .NET ?

Creator
Creator

You can try to call PS command, and automate the selection file dialog.

TxApplication.CommandsManager.ExecuteCommand("EMServer.ImportEBOPFromFile");