Cancel
Showing results for 
Search instead for 
Did you mean: 

is it possible to create any TxPlanningObject using sdk ?

Experimenter
Experimenter

i try to create  TxPlanningObject  in the process designer, for example operation or resource.

 20170710160300.jpg

 

it works in process simulate,but not in the process designer.is any one meet the same question? thank you

1 REPLY 1

Re: is it possible to create any TxPlanningObject using sdk ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Dlat333,

 

I am looking at the code, you select two existing objects and try to add one as a child of the other.

What is the type of the selected objects and which part of the code does not work?

 

The SDK provides API that works only for loaded data, this means that you need to have study or cell loaded.

If you want to create a part or resource instance, please check this example.

 

Best Regards,

DianaG