Cancel
Showing results for 
Search instead for 
Did you mean: 

Excel-based model generation

Community Manager Community Manager
Community Manager

 

As we had a question for Excel-based model generation, here is an example of how to do it

 

  • Read data from an Excel file
  • Create a new conveyor in Plant Simulation and how to
  • Set the parameters in the segment table for the conveyor
  • You have to save model file and Excel file in the same folder
  • If you have questions, please contact Matthias.heinicke@siemens.com

 

Tangential angle Length Curve angle Radius Vertical curve ΔZ    
          0 2 -4
45 3       0    
0   45 7 FALSE 0    

 

Kind regards

Matthias.Heinicke@siemens.com

Comments
Experimenter
Experimenter

I have tried and it is a good example. There are two notes:

1. The model was created with Plant Simulation 14.2. The latest Plant Simulation software is needed

2. The downloaded Excel file name is Segments2 (003).xlsx. Change to Segments2.xlsx at first

 

 

Enthusiast
Enthusiast

any one please share some more examples related with simulation in plantsim using excel only.

 

thank you,

 

Yogesh1