Cancel
Showing results for 
Search instead for 
Did you mean: 

High Quality Movie Capturing with Robot Expert 11

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

I have the Movie Capture feature integrated in oRobot Expert 11.
It actually works!
Oddly, jerky video when recording. (see video)
Robot Expert in the Path does not wobble.

 

 

(view in My Videos)

Kind regards,

Benjamin Voelzke
Comments
Experimenter
Experimenter

Very nice. How do you synchronize the devices/robots?

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

i synchronize the robot's over signals.

in robot expert you can work with Signals.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Ben,

right...the wobbling is strange and should not happen.

 

Are you moving the cam as robot or flow? If robot: best result with linear movement.

 

Does it disappear when you switch to 5DOF? (checkbox in properties of MovieCapture)

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Very very very nice!

I have to talk to you guys - how did you do it? (the camera path)

I'd like my Robot Expert QA Solution engineers to create such nice movies for the new functionality we are developing here to share the new stuff on this site. Would that be helpful?

 

Appreciate the help,

Yuval Maimon

Development Engineering QA TL

Contributors