Cancel
Showing results for 
Search instead for 
Did you mean: 

Unresolved DRF Gage Size

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

In Variation Analysis, when validating or initialing a model for simulation, the following message may appear:

 

Unresolved DRF Gage Size.png

 

This message indicates that there is a datum reference frame with one or more datum features of size that the software cannot automatically determine the gage size for simulation during feature fabrication.  The following video provides further information on the meaning behind this message and how to calculate & apply the gage size for these cases. 

 

(view in My Videos)

 

Note that this message is not an error and is merely a warning.  The error message is to a changed warning in patches 11.3.0.1_a01_7 & 11.5.0.5 and in releases 11.6 & 12.1.  If gage size(s) are not explicitly specified, the warning can be ignored and the software will make an assumption on the gage size.