Cancel
Showing results for 
Search instead for 
Did you mean: 

ABB Download whitout Process Data

Pioneer
Pioneer

Hello Guys,

 

Is there a way to download a path usign ABB controller whithout showing the Spot Data, Speed Data, Zone Data and Gun Data declareted in the begin of the program?

 

I need to use these  configureteds Data but I dont want then in the upside of the downloated module.

 

I created a MotionConfiguration (used to edit the name of weld instruction) that could be useful to do it, maybe creating a custom parameter... but the idea is to use the most default parameter of abb controller (that is necessary to simulation e behavior of robot ) and use the motionconfiguration just to change a dowload. 

 

 

1 REPLY

Re: ABB Download whitout Process Data

Siemens Phenom Siemens Phenom
Siemens Phenom

You just need to write those global data definitions in a .sys file, then import this .sys file via Robot Setup / Explicit Data Upload.

These global data will be available in Robot Setup Data Edition read-only, you can assign them to locations, but their definitions will not be written down in the program file.