Cancel
Showing results for 
Search instead for 
Did you mean: 

Apply Path Template - SPOT

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everybody,

 

is it possible to use Apply Path Template just for spot weld point? (e.g. using some kind of filter)

 

What I need to do:

 

I have SpotWeldOp consisting via and spot locations and I would like to set some parameters of spot welds only.

 

 Clipboard01.jpg

 

My Action works, but it throws an error, because the via locs do not have Thickness and Schedule parameter.

 

		<Action Name="SPOT_Th_1_Ti_1" Description="Sets Spot Thickness=1mm and Spot weld schedule = 1s">
			<Param Name="Thickness" Dynamic="True" Value="1"/>                    
			<Param Name="Schedule" Dynamic="True" Value="1"/>
		</Action>

 

Thanks in advance

 

Dave

 

 

2 REPLIES

Re: Apply Path Template - SPOT

Valued Contributor
Valued Contributor
<Action Name="SPOT_Th_1_Ti_1" LocationTypes="WELD" Description="Sets Spot Thickness=1mm and Spot weld schedule = 1s">
			<Param Name="Thickness" Dynamic="True" Value="1"/>                    
			<Param Name="Schedule" Dynamic="True" Value="1"/>
		</Action>

 

I think that´s what you want. Smiley Wink

 

You can also use ProcessTypes="yourcustomprocess" or MotionTypes="1,2" (1 is lin, 2 is joint afaik) to filter out what you want.

Re: Apply Path Template - SPOT

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

That's it!

 

Thanks a lot

 

Dave