Cancel
Showing results for 
Search instead for 
Did you mean: 

Are there plans to integrate FANUC linetracking in PS 13.0?

Experimenter
Experimenter

Hello,

 

in the Fanuc Teachpendant ChangeLogs there are some hints that PS supports line tracking with FANUC robots.2016-06-21 13_14_20-Fanuc-Rj.png

2016-06-21 13_15_30-Mozilla Firefox.png

In the robot setup there is a button called "Line Tracking Settings".

I would like to get some more detailed information about development regarding FANIC line or railtracking with PS

 

Kind regards

1 REPLY 1

Re: Are there plans to integrate FANUC linetracking in PS 13.0?

Siemens Phenom Siemens Phenom
Siemens Phenom

Correct, this is currently under investigation. No firm plan however.