Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't select lines like of frames in Graphics Viewer on high-DPI display

Creator
Creator

Hi,

Since upgrading to a 4k display I can no longer click to select lines in the Graphics Viewer unless there is nothing selectable in the background behind it. I'm refering to lines like what makes up a frame or the location manipulator. I've moved the mouse in 1 pixel increments across a line trying to select it to confirm that I'm not just missing it. The background object always gets selected. If there is no background object, then I can easily select the line even when I'm off by a few pixels.

 

Is there any way to increase the selectable padding around a 1 dimmensional entity?

 

Running ProcessSimulate 13.0

1 REPLY 1

Re: Can't select lines like of frames in Graphics Viewer on high-DPI display

Creator
Creator

I found a workaround. Toggling "Show Locations/Frames Always on Top" on and off fixes... something and alows me to select lines with objects behind them again.