Cancel
Showing results for 
Search instead for 
Did you mean: 

Contimuous Process Generatror

Experimenter
Experimenter

I am using continuous process generator to create MIG Weld Seam in Process simulate13.1.

I observed once weld seam created It cannot be sequenced (Related to Direction.)

For example weld seam from point A to Point B. I want to make reverse direction. In path editor it is not showing "move up/move down" applicable.

Is there any way to re-arrange them?

 

Refer Image;

1 REPLY 1

Re: Contimuous Process Generatror

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

You cannot change the order of seam locations within a seam.

You need to "reverse the operation". There is a function to fully reverse the locations within the seam.

so your last location will be the first and the first will be the last.

 

Best regards

Patrick