Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Create cable - RobotExpert

Experimenter
Experimenter

Hello,
I have found information, that since version 13, Robotexper can also simulate robot cables. I have version 13.1.2 but I can not find a way to make cables.
How I can do it?

Regards, Tomas.

1 REPLY 1

Re: Create cable - RobotExpert

Siemens Phenom Siemens Phenom
Siemens Phenom
If Cables are enabled in RobotExpert, you may need to add the commands into the Toolbar using the customize option if they are not already included. The cables commands in Process Simulate are located in the Modeling tab of the Toolbar. In Process Simulate, cables are an extra licensed option.