Cancel
Showing results for 
Search instead for 
Did you mean: 

Custom OLP commands UILayer

Valued Contributor
Valued Contributor

Hi

 

I am trying to find out a way in the OlpConfiguration file in the UILayer to force the command to be displayed over multiple lines. See below this is what I have to far

 

<UILayer>

         <Line>

           <Item Type="parameter">commentPrefix</Item>

         </Line>

         <Line>

           <Item Type="const">;WELD SEQUENCE COMPLETE</Item>

         </Line>

         <Line>

           <Item Type="const"> SIGNAL</Item>

           <Item Type="parameter" Default="447">sig_num</Item>

          <Item Type="const">; WELD SEQUENCE COMPLETE</Item>

         </Line>

         <Line>

           <Item Type="parameter">commentSuffix</Item>          

         </Line>

       </UILayer>

 

I thought placing each <item> in a separate <Line> but this does not seem to work. I know this must be possible because the drivedrive does it in one command as below.

 

# Destination bx200l_a001_a_3

# Drive HOME

 

 Thanks

3 REPLIES

Re: Custom OLP commands UILayer

Siemens Phenom Siemens Phenom
Siemens Phenom

You need to create 2 single lines Olp Commands and embed them in a single OlpDialog. The 2 lines will then go together (selected together, edited together).

Re: Custom OLP commands UILayer

Valued Contributor
Valued Contributor

Great thanks for the help

Re: Custom OLP commands UILayer

Creator
Creator

Hello,

 

I know this is an old thread, but I was wondering if you could explain how/what you mean by "embed them in a single OlpDialog." I thought the OlpDialog was only used for the Menu display. 

 

I tried multiple ways, but still cannot get the OLP's to display on multiple lines.