Cancel
Showing results for 
Search instead for 
Did you mean: 

Customized OLP-Command is not written in the program

Creator
Creator

Hello guys,

 

I created a customized OLP-Command-Dialog with this schema:

 

! --------- ;

! --------- ;

! Comment ;

! Comment ;

! Comment ;

! Comment ;

! --------- ;

! --------- ;

UFRAME_NUM=X;

UTOOL=X;

PAYLOAD[X];

 

 

I created the dialog in the *.xml and Im able to configurate the params in Process Simulate.

It is also displayed in the Path-Window, but when I download the program onto the robot, the commands are not written in it.

 

The Command refers to the root-op and is not connected to a location. When I write the commands manual with free text or with the tools in the OLP-dialog it is written in the program.

 

Is there a solution for it?

 

Best regards

 

Max

 

 

 

 

4 REPLIES

Re: Customized OLP-Command is not written in the program

Siemens Phenom Siemens Phenom
Siemens Phenom

Did you properly implement a <DownloadLayer> in your xml? What is displayed in the Teach Pendant is the <UILayer>. What is written down in the program is the <DownloadLayer>.

Re: Customized OLP-Command is not written in the program

Creator
Creator

Ok I see, there is the problem. I didn't know that i also had to connect the UILayer to the DownloadLayer. I think the schema from is the same as in the UILayer?

Re: Customized OLP-Command is not written in the program

Siemens Phenom Siemens Phenom
Siemens Phenom

The important part for you is the <DownloadLayer> as it is what you want to see in the program. For the <UILayer>, you may prefer a simplified version of the command(s) (for instance, a single line "MyHeader").

Re: Customized OLP-Command is not written in the program

Creator
Creator

Yeah, thats it. Thanks for that.

 

Best Regards

 

Max