Cancel
Showing results for 
Search instead for 
Did you mean: 

Customized Path Template in Simulate

Creator
Creator

Hello,

 

is it possible to create an interlaced action in a customized template?

 

I want to place some olp-commands for the first via location and all weld locations in one task.

 

For example:

 

<Action Name="Parent Task" LocationTypes="VIA" LocRange="First>

   ...

   <Action Name="Child Task" LocationTypes="WELD" LocRange="ALL">

      ...

   </Action>

</Action>

 

If I do so, i get an error message.

 

Is there any solution for it?

 

Best Regards

 

Max Gropp

 

 

 

 

7 REPLIES

Re: Customized Path Template in Simulate

Siemens Legend Siemens Legend
Siemens Legend

Hello Max

 

you cannot have interlaced actions.

 

the solution for this is following:

- create an action for the weld locations action1

- create another action for the via locations action2

- create another action (action3) that references the 2 actions (action1, action2)

 

from the path template, you select action3

 

best regards

bernard Hoessler

Re: Customized Path Template in Simulate

Creator
Creator

Thanks, it works very well.

 

But i have another question, is it possible to create one point before and after a weld-location with an offset of z=-10?

 

Thank you!

 

Best Regards

 

Max

Re: Customized Path Template in Simulate

Siemens Legend Siemens Legend
Siemens Legend

Hello Max,

 

yes, that is possible as well.

in the spot action, use AddLoc command, you can specify type (via) before or after and offset. Currently ofsset can only be relative to the reference location.

To create locations before and after, you need to use 2 AddLoc commands in the same action.

 

best regards

Bernard

 

Re: Customized Path Template in Simulate

Creator
Creator

Awww, thats great!

 

I will check that out right tomorrow!

 

Thanks for that. If there are any more questions I will ask them here.

 

Thanks for the great help!

 

 

Best Regards

 

Max

Re: Customized Path Template in Simulate

Creator
Creator

So Bernhard, this also works very well!

 

Thanks for that.

 

I have one last question for the moment, is there a reverse command for AddLoc?

 

The thing is, if i accidentally create locations via the AddLoc command to delete a location before and after the weldlocation?

 

Greetings

 

Max

Re: Customized Path Template in Simulate

Siemens Legend Siemens Legend
Siemens Legend

Hello Max,

 

no, there is no opposite action to the AddLoc.

 

However, if you realize after applying the path template that something is wrong, you can use "undo". This will cancel all channges applied by the path template.

 

best regards

Bernard

Re: Customized Path Template in Simulate

Creator
Creator

Ok too bad that there is no such command, but then my collegues have to take a closer look for what they are doing Smiley Wink

 

Thanks for the great support bernhard!

 

Merry Christmas and happy new year.

 

Best regards

 

Max