Cancel
Showing results for 
Search instead for 
Did you mean: 

Does Process Simulate support G-Code?

Experimenter
Experimenter

I have an automated system which reuqires G-Code to operate. I was wondering if I can create offline programs for the system in Process Simulate for virtual commissioning purpose. If not, can we use any other platform to write the G-Code and then connect that to Process Simulate via OPC to simulate operations?

Thanks.

4 REPLIES

Re: Does Process Simulate support G-Code?

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, with NC-Code controller.

Re: Does Process Simulate support G-Code?

Experimenter
Experimenter
Thanks for your reply. Can you please elaborate that? I am not sure where can I access NC-Code controller. Is that like an RCS that I need to setup within Process Simulate?

Re: Does Process Simulate support G-Code?

Siemens Phenom Siemens Phenom
Siemens Phenom

You need to download the NC-Code controller from GTAC, install it and then assign "NC-Code" controller to your robot/machine.

Re: Does Process Simulate support G-Code?

Experimenter
Experimenter
Thanks!