Cancel
Showing results for 
Search instead for 
Did you mean: 

Downloading plain text program to Process Simulate

Pioneer
Pioneer

Hello to experts,

There is such a command in PS as "Download a program to robot" which creates a plain text source file. Suppose I manually edited this file or data file. How can I get it back to a study to run a simulation? I see there is a command "Upload a program" but I don't get how it works ((.

3 REPLIES

Re: Downloading plain text program to Process Simulate

Legend
Legend

If you use the "Upload Program" command in "Program Inventory" it should work!!!

(Robotic -> Robotic Program -> Robotic Program Inventory)

 

But if it is not a robot program with the correct syntax of robot vendor, the upload does not work!

Re: Downloading plain text program to Process Simulate

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello guys,

 

I have the same problem. The button Upload Program is not active.

I haven't tried with other RCS or Controller, but for the default it certainly doesn't work.

The Upload Robcad Robotic Program is working, but what I need is to download a program from PS with the default controller and then upload it back in PS for the default controller.

Is there a way around this?

Thanks.

Re: Downloading plain text program to Process Simulate

Siemens Phenom Siemens Phenom
Siemens Phenom

Unfortunately "Upload" for default controller is not supported yet. You need to use a real controller instead.