05-11-2016 10:14 AM - edited 05-12-2016 06:46 AM
Hey,
I'm trying to monitor the power consumption of Robots in Process Simulate using a RCS Module by Kuka.
The Module itself is working, the issue I have concerns the power consumption monitor in the Robot Viewer.
I'm using a Kuka KR500_2 Robot with a krc8.3_r14 RCS Module. When I simulate a movement it says "unsupported service for current rcs version".
When asking Kuka they told me to configure the machinedata in WorkVisual. I did so but nothing changed.
Does anyone have an idea what the problem is?
Thanks so far,
Felix
Solved! Go to Solution.
05-25-2016 07:18 AM
problem solved it simply did not work with the robot is used.
05-30-2016 02:05 AM
Hi FS_ZeMA
Thanks for posting the answer !
Please be aware that Kuka RCS Energy has another issue: the Machine Data itself does not include the information of whether or not it includes Energy, so PS can't tell whether it does or does not. This means that if you try to monitor a robot who's MADA does not include Energy, you might still see some values in the Robot Viewer which will be misleading (usually it's easy to tell since the values shown will be very wrong and the chart will be very jittery).
05-30-2016 04:49 AM
Thanks for the reply,
could you try to solve my second problem i postet last week? I have some graphs in the robot viewer but they are wrong.
Regards,
Felix
Watch Replays of Previous Topics