Cancel
Showing results for 
Search instead for 
Did you mean: 

Error RCS module of the FANUC

Valued Contributor
Valued Contributor

Hello guys!

 

I would like to know how to proceed when creating a virtual robot.

 

Because I create it according to the model, and enable the RCS, but at the time of running the motion programs it generates this error:

 

[R7_r2000ib_210f_so_le][RRS][203.20][Error] (T_Z3_F3E) P1: Motion Failed: Fatal error. Stopped calculating GET_NEXT_STEP service., Error Code: -68

 

Which error -68 is this?

4 REPLIES 4

Re: Error RCS module of the FANUC

Siemens Phenom Siemens Phenom
Siemens Phenom

It is a motion planning error from the RCS (like attempting to cross a singularity in linear motion, robot joints exceeding limits during motion, etc...).

Re: Error RCS module of the FANUC

Valued Contributor
Valued Contributor

Ok, I'll check the movements better.

Highlighted

Re: Error RCS module of the FANUC

Experimenter
Experimenter

This error is from virtual robot Fanuc , need inclued itens , like a photo

Parametros virtual robot.PNG

 

 

Re: Error RCS module of the FANUC

Pioneer
Pioneer

That error is often triggered by mfg features not being assigned to the proper appearance. Turn on the visibility of the operation that is running when the error occurs. If the mfgs are at zero, you have issues with your material flow.

 

Also, do you have at least 3 vias before the weld (If it is a weld path)? FANUC RCS is scanning ahead three tags.

 

Basically the error is saying that your robot can't reach it's target.