Cancel
Showing results for 
Search instead for 
Did you mean: 

Event simulation without PLC

Pioneer
Pioneer

Hello,

does anyone know about possibility to start Event base simulation without PLC or any additional HW?

Maybe there is a way to "trick" PS, that there is connection?


Thanks for help in advance

2 REPLIES 2

Re: Event simulation without PLC

Siemens Phenom Siemens Phenom
Siemens Phenom

Not sure I understand you correctly...

At Options>>PLC tab you can switch between internal (CEE) and external (PLC) event-engine.

The shouldn't be any "tricks" needed ;-)

Re: Event simulation without PLC

Pioneer
Pioneer

Thank you for reply,

The thing is:
1. I don't want to work with CEE
2. I want to start external connection without any PLC program, PLC controller or Simba (only for simulate to work in this mode, whatever which one). There is functionality that i want from this mode.