Cancel
Showing results for 
Search instead for 
Did you mean: 

Exporting/getting external axes values

Siemens Creator Siemens Creator
Siemens Creator

Hi all,

 

I've got robot with defined external axis (positioner, 1 axis) and i want to use values of positioner in OLP Command window.

I have read in Default Controller Manual that I have access to some variables of robot, like present position of TCPF by writing in OLP Command window ${Robot.TCPF.X}. Also i found that there is a class that represents an external axes and it is called ExternalAxes. I have tried many combination like:

${Robot.ExternalAxes}

${Robot.ExternalAxes.value}

${Robot.ExternalAxes.j1}

 

none of them works.

 

Can somebody help me with this?

Thanks in advance.

 

1 REPLY

Re: Exporting/getting external axes values

Siemens Phenom Siemens Phenom
Siemens Phenom

You should use dynamic parameter "Ext1" (see in Path Editor, in Olp section) in a custom olp command (see pdl manual under eMPower\Robotics\Olp).