Cancel
Showing results for 
Search instead for 
Did you mean: 

FUPA from Robcad

Pioneer
Pioneer

Is it possible to attach the KUKA fupa for quantec robots from robcad to the robotexpert model

 

The import works and all joint are in the jtco.

 

 

best regards

4 REPLIES

Re: FUPA from Robcad

Legend
Legend

in this post may you can find some information what you are searching for.

 

http://community.plm.automation.siemens.com/t5/Tecnomatix-Robotics-Forum/Upgrade-CO-to-version/m-p/2...

Re: FUPA from Robcad

Siemens Legend Siemens Legend
Siemens Legend

Hi Robolab.

I don't think you can.

You can upgrade a SuperComponent to a .co (as Patrick's mentioned thread discusses), but it isn't possible to upgrade them to the RobotExpert's required .cojt.

 

Sorry,

 

 

Kind regards,
Gal Snir

Re: FUPA from Robcad

Pioneer
Pioneer

Is it possible to attach the fupa to the robot model and set an kinematic following?

Re: FUPA from Robcad

Siemens Legend Siemens Legend
Siemens Legend
Hi Robolab.
A Following joint can only follow a joint of the same component, so you would have to effectively copy one component into the other and redefine the copied components kinematics and such, which can be a handful.
In Process Simulate you can set a "Coupling" relation between joints of different components which are nested under an Equipment Prototype, but it is not supported in RE (Equipment I mean).
Kind regards,
Gal Snir