Cancel
Showing results for 
Search instead for 
Did you mean: 

Fatal Error

Experimenter
Experimenter
Hello,

I just installed the 30 days trial of RobotExpert.
But the first message I get is "Fatal Error: Access Violation", and the program don't launch. (After a fresh install)

The computer is : i7-2600K, Quadro 2000 (306.79), 16Go DDR3-1333, Seven Pro 64b SP1.
I usually use this computer without any problems for Autocad and NX 7.5.

Anyone know if there is a solution ?
Thank you.
2 REPLIES 2

Re: Fatal Error

Experimenter
Experimenter
Solved ...
If you not install on C:\Program Files\Tecnomatix, it crash, and you need to run TecnoReg.exe manually ...

Re: Fatal Error

Not applicable
I also have the same error when I try to run the 30 trial version. I have the program installed in the C:\Program Files\Tecnomatix\eMPower directory. Are you suggesting that TecnoReg.exe will solve my problem?