Cancel
Showing results for 
Search instead for 
Did you mean: 

Grouping of WeldLocations?

Valued Contributor
Valued Contributor

Hi everyone,

I´m using PS & PD 10.1 Standalone. Smiley Wink

I have imported several weld locations via .csv,´s an grouped them in different mfglibraries.

When I drag the libraries into my RobCadStudy, all weldpoints are under the root tree, but without any groups.

Is there any posibility to import them like they are grouped together?

4 REPLIES

Re: Grouping of WeldLocations?

Pioneer
Pioneer
You can group them in different weldoperations and then look them up in the relations viewer. Do that do the job?

Re: Grouping of WeldLocations?

Valued Contributor
Valued Contributor

That´s possible, but awkward.

 

What I mean is to take over the groups from MFG-Libraries.

 

Re: Grouping of WeldLocations?

Pioneer
Pioneer
I would again say you should group them in weldoperations. Then they will be grouped nicely in the operation tree.

That can also be done through the csv file. Then have your weldoperations in the study and not the mfg library.

And even maybe group the weldoperations in compound processes and stationprocesses.

If you still think this is awkward you have to give some better arguments why this is awkward.

Re: Grouping of WeldLocations?

Experimenter
Experimenter

Hi,

try this.

Cretae SWP and then drag the points in.