Showing results for 
Search instead for 
Do you mean 
Reply

Help of PS 11.1 with Step7 5.5 sp4

Hello Expert,
I install ps11.1 and Step7 5.5 sp4, but when I use the plcsim, it is grey so I feel very weird.
the operation procedure is as following,
tools->option->PLC tab->plc, but the plcsim tab is grey and I can't click it.
please help me about.it.

best regards
Paul
2 REPLIES

Re: Help of PS 11.1 with Step7 5.5 sp4

Hi Paul,

hard to tell from here, but you definitely have to make sure, that if you have PS 64bit version, your PLCSim must be 64bit as well.

Here is a thread dealing with this topic, but the guy who made it work was already using 11.1TR3, your version is more than 3 years old.

You may contact GTAC, for further information, but as v11.1 is already out of maintanance, they might tell you to upgrade to a never version.

 

 

 

Re: Help of PS 11.1 with Step7 5.5 sp4

Hi Guido,
Thanks for your reply.

Paul