Cancel
Showing results for 
Search instead for 
Did you mean: 

How to create continuous circular motion of disk using logic blocks ?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter
 
3 REPLIES 3
Highlighted

Re: How to create continuous circular motion of disk using logic blocks ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

I think you have to explain this more in detail.

What has a circular motion to do with an LB.

 

If you want to rotate something, you need to create a device with a joint and inside the LB you can use the actions.

 

Best regards

Patrick

Re: How to create continuous circular motion of disk using logic blocks ?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi,

i have circular disk which is contionously rotating amoung which having four cavities.

at each cavity robot place a part ,but disk is continously rotating with less speed.

  I am trying to write the logic block for this robot action along with disk cavity positions.for cyclic simulation.

 

Re: How to create continuous circular motion of disk using logic blocks ?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

 Hi