Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: How to handle material flow and part appearance in CEE

Creator
Creator

Ok! i understand it! the only thing that is not working is to make a set reset with more conditionsSmiley Happy

 

ex:

 

SR ( (inputA or InputB) InputC )

 

set conditions are A or B

reset is C

 

 

Re: How to handle material flow and part appearance in CEE

Siemens Phenom Siemens Phenom
Siemens Phenom

You are right.

Your need to add an extra signal

mem1=inputA or InputB

SR(mem1 inputC)

Re: How to handle material flow and part appearance in CEE

Pioneer
Pioneer

Hi,

 

For logic like that I prefer to use Parameters inside of LB. Thanks to that there is no need for more signals and when project is big it's making difference.

Re: How to handle material flow and part appearance in CEE

Pioneer
Pioneer
Hello Ushan,
I also encounter the same problem, I hope you can share with me about the video in youtube (which is private)so I can learn from you about how to solve.the same problem.
thanks in advance.

best regards.
Paul