Cancel
Showing results for 
Search instead for 
Did you mean: 

How to import .JT to Process Simulate?

Experimenter
Experimenter

I am new to Process Simulate and I need to simulate a manufacturing cell I made on CAD, but i can't grasp on how to import my .jt file to use it in Process Simulate.

 

Thanks in advance!

17 REPLIES 17

Re: How to import .JT to Process Simulate?

Siemens Genius Siemens Genius
Siemens Genius

Assuming you ue Process Simulate on eMServer, you can use the "Import CAD Files" command.

It is available from the Navigation Tree ( File menu).

 

Re: How to import .JT to Process Simulate?

Experimenter
Experimenter

I did that, but an error message that says that the xml file could not be created appears, what should I do to correct that?

Re: How to import .JT to Process Simulate?

Siemens Genius Siemens Genius
Siemens Genius

Strange. It should work. Do you have a problem with any JT file, even a simple one?

Which PS version do you use?

Gil.

Re: How to import .JT to Process Simulate?

Experimenter
Experimenter

I´m using PS 11.0.2, and that problem doesn't appear with simpler files.

Re: How to import .JT to Process Simulate?

Creator
Creator

Dear all,

 

Could you tell if I can import gun and robot ft data into process simulate. I execute the program standalone and i could not find a way to import jt file and also i could not manage to import the.co robcad file that includes kinematic stuff  into process simulate.

 

As i importing the file i get a error like in attachments.

 

Could you send me file step bt step importing, it would be great.

 

Thanks in advanced

Re: How to import .JT to Process Simulate?

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

good morning,

 

you can import CAD Files via CAD import function. (show customize)

before you import *.cojt file to your cell please delete the tunedata.xml under *.cojt folder.

 

with CAD import function creates a new tunedata.xml file.

 

after the CAD import function you can import the 3d file (*.cojt) via "insert component from file"

 

Please check you systemroot.

you can only insert 3d files under system root.

 

Kind regards,

Benjamin Voelzke

Re: How to import .JT to Process Simulate?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

PS Standalone uses library on the local disk. You should set the library folder first. So:

 

1. Tools - Options - Disconnected - Client System Root

Set the folder here

2. For data import use UpgradeToVersionWin utility. It can be found in the PS instalation folder (e.g. C:\Program Files\Tecnomatix_12\eMPower)

3. Then you must use Define Component Type Command in PS.

 

Dave

Re: How to import .JT to Process Simulate?

Creator
Creator

hello

i have problem with importing file. could you please help me with importing .stp file to process simulate.

how can i import .stp file to process simulation.

thank you

Re: How to import .JT to Process Simulate?

Legend
Legend

You cannot import .stp files to PS.

You have to convert the .stp file to a .jt file first.

 

This can be done with the Cad translators or a 3rd party program.