Cancel
Showing results for 
Search instead for 
Did you mean: 

How to import .pgz to PS Standalone eMServer Compatible?

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello,

I have a PGZ file to import but no database setup. I usually work with disconnected studies. Since the PS version is called eMServer Compatible is there any way to setup the eMServer and import such a project? The Pack and Go import is currently inactive.

1 REPLY 1

Re: How to import .pgz to PS Standalone eMServer Compatible?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

You need a eM-Server database to be able to import the PGZ File (Pack&Go Export) into your environment.

Therefore, you need to create a new project and run the Pack&Go Import.

 

Disconnected called eMS-Compatible, because the PSZ file is coming from an eMS database or was created based on eMS.

There are also disconnect studies for Teamcenter environment (PSZ-TC). These files are only TC-Compatible.

 

Best regards

Patrick