Cancel
Showing results for 
Search instead for 
Did you mean: 

How to set TCP maximum default robot

Valued Contributor
Valued Contributor

Hi

 

I have created a 3 axis robot which I would like to set the maximum TCP speed. I have set the value in the path editor to what I would like but it does not follow this speed above a certain amount, I think it must be a maximum speed limit. I have also tried to set the speed and acceleration to large values in the kinematic editor to see if this would help and it does not. Where would I set this?

 

Also I have used the robot viewer to track this speed and I can see that it is being limited

 

Regards

1 REPLY 1

Re: How to set TCP maximum default robot

Siemens Phenom Siemens Phenom
Siemens Phenom

Please look at motionparameters-e.pdf under eMPower\Help\Additional Reference Material.