Showing results for 
Search instead for 
Do you mean 
Reply

Idependant Joint Poses In a Single .cojt model with 2 or more Joints/Clamps

My issue regards Process Simulate. I have a single .cojt model with 2 clamps. Each clamp has its own joint. I need to pose each joint/clamp independently from the other. How can I create a pose which only defines a single joint steering/poses position and leave the other joints where they are?

 

For now this is a simple model, but I do have more .cojt models that include more clamps and other devices which will also need independent poses.

2 REPLIES

Re: Idependant Joint Poses In a Single .cojt model with 2 or more Joints/Clamps

if you have two joints.

create a pose where one joint is open and the other one is closed.

if you want a pose with both opened, move both joints to open and create a pose.

 

regards

 

Patrick

Re: Idependant Joint Poses In a Single .cojt model with 2 or more Joints/Clamps

Other solution is splitting the component.
-Take clamp into modelling
-copy it, to create a new prototype
-‎remove in both comps the opposite part


-----------------
Siemens Industry Software GmbH & Co. KG; Anschrift: Franz-Geuer-Str. 10, 50823 Köln;
Kommanditgesellschaft: Sitz der Gesellschaft: Köln; Registergericht: Amtsgericht Köln, HRA 28227;
Geschäftsführung und persönlich haftender Gesellschafter: Siemens Industry Software Management GmbH;
Geschäftsführer: Urban August, Daniel Trebes; Sitz der Gesellschaft: Köln; Registergericht: Amtsgericht Köln, HRB 70858