Cancel
Showing results for 
Search instead for 
Did you mean: 

Import jt-file in standalone Process Simulate dosen't work

Experimenter
Experimenter

JT import doesn't work in standalone Process Simulate. Here some Pictures:

simualte_1.png

simulate_2.jpg

simulate_3.png

 

Someone any idea ?

2 REPLIES

Re: Import jt-file in standalone Process Simulate dosen't work

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

this dialog requires the CadTranslators to be installed.

Are they?

The setup lies next to the PS setup on GTAC-Server.

 

Btw: if you just want to load a monotlitic JT-file, there is no need to translate.

1. Set your sysroot-path

2. add a folder xyz.cojt under sysroot and put your JT-file into it

3. use button "Define Component type" in PS to set the required class on your part

Now you can D&D it into your study.

 

Re: Import jt-file in standalone Process Simulate dosen't work

Experimenter
Experimenter

Yes, we have installed the CadTranslators.

Must we configure something in PS to use it ?