Cancel
Showing results for 
Search instead for 
Did you mean: 

KUKA KRC BMW OLP Command "Fold Stamp Comment Commands"

Legend
Legend

How to add a new "Fold Stamp Comment Command" into a robot program? (see pic)

TimeStamp.jpg


After an upload which includes the stamp, I am able to edit it but if it is not available from the upload, I cannot add a new one. I can´t find it in the custom XMLs for KUKA BMW.

 

Is this a hard coded function or is it a custom function?

4 REPLIES

Re: KUKA KRC BMW OLP Command "Fold Stamp Comment Commands"

Siemens Phenom Siemens Phenom
Siemens Phenom

It is in the "Misc" section, but only for Controller Version 8.3 and above.

Re: KUKA KRC BMW OLP Command "Fold Stamp Comment Commands"

Legend
Legend

ok thanks for the information.

 

But we actually use kuka krc 5.5 (krc2).

With a double click on the available line in the OLP command I can edit the stamp. So the menu is available, but I am not able to create a new one if the function is not availbable in robot path.

Re: KUKA KRC BMW OLP Command "Fold Stamp Comment Commands"

Siemens Phenom Siemens Phenom
Siemens Phenom

Does this command already exist in 5.5 in Kuka Office? This command is editable whatever the version, but is available in the Misc list only for 8.3 right now...

Re: KUKA KRC BMW OLP Command "Fold Stamp Comment Commands"

Legend
Legend

I don´t know if the command is available in 5.5 Kuka Office.

 

Ok. Thanks for the information.