Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Kuka RCS Installation

Valued Contributor
Valued Contributor

Hello.

Can you help me with instalation RCS module for Kuka krcs 8.3/8.2.

Please describe all process step by step, if it isn't difficult.

 

Now i already do it this:

 

1) download

rcs_kuka_WIN_krc8.3_r14.00_09.05.2014_PC. zip,

rcs_kuka_WIN.83.TuneAddOn.16_11_2015_PC.zip,

KRC4-KSS_83_b105_RRS1Structure.zip 

from Siemens PLM Download Server.

 

2) change the rrs.xml for this:

<?xml version="1.0" standalone="yes" ?>
<Data>
<ControllersData>
<Controller Name="Kuka-Krc">
<InstalledVersions>
<Version Name="8.3">
<ModuleName>C:\cad\Tecnomatix_12.1.3\RCS module Kuka\rcs_kuka_WIN_krc8.3_r14.00_09.05.2014_PC\rrs_bin\rcs_krc1\krc8.3_r14\bin\rcskrc1_tune.exe</ModuleName>
<!--ModulePathName is not mandatory in PS-->
<ModulePathName>ENTER HERE: The full path to the rcs module path (for this version)</ModulePathName>
</Version>

</InstalledVersions>
</Controller>
</ControllersData>
</Data>

 

3)select RCS version in this menu:

  RCS.PNG

 

But when i am trying to simulate process emerge next errors:

- The RCS-Module could not be initialized. Reason: The ModuleName specified in rrs.xml file, doesn't exist.
- The RCS-Module for the Kuka-Krc controller, could not be initialized - srez_0 was simulated disconnected from RCS.

 

I'am using Process Simulate v.12.1.3 and my robot is Kuka quantec Kr 300 r 2500 ultra foundry

6 REPLIES 6

Re: Kuka RCS Installation

Genius
Genius

Hi,

 

  Please note: Not all module of robot ( KUKA/ABB) in Tecnomatix can be used to do RCS OLP simulation. Look at the content in .co or .cojt files. Does it contain sub folder called .rrs ? if no. it would not be able to do RCS simulation since manipulator info are within .rrs folder. this is why you can't see in your PS command.  

 

  You can easily compare those robot models who had .rrs folder and those don't have. see the difference. maybe for the reason of popularity of models to be used. some of them have, but some others don't. 

 

Steve

Re: Kuka RCS Installation

Valued Contributor
Valued Contributor

Hello. My problem in installation kuka rcs is spaces in directory with rcs. When I correct this mistake our module is validate.

 

rcs module.PNGBut i don't understand why the RRS folder is needed. I download robot from kuka web site and download KRC4-KSS_83_b105_RRS1Structure from Siemens PLM Download Server. Then I choose R1, Steu, config folders in controller settings and connect with rcs.

Currently I dont have result because i have got some problems with license file. When i get a new license - i'll report you.

 

Re: Kuka RCS Installation

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Have you uploaded MADA before the initialization of the RCS?

Re: Kuka RCS Installation

Valued Contributor
Valued Contributor

No.

I'am loaded only machine Data. Our files are taken from KRC4-KSS_83_b105_RRS1Structure.Снимок.PNGMada is loaded from Robot backup.

Снимок2.PNG

Re: Kuka RCS Installation

Genius
Genius

I think you need to load MADA data ( R1/Stu/Config) from MADA folder before testing connection.

if license ok. it will run. but you need to make sure the data in MADA folder is correct one referring to the model in PS. 

Re: Kuka RCS Installation

Valued Contributor
Valued Contributor
Ok. I'll try.