08-12-2015 11:25 AM
Hello
What do I have to do for add a external axis to a simulation with rcs KUKA on?
My problem is that when I run the path with RCS the gun does't move.
Thanks
08-12-2015 11:28 AM
you need dedicated machine data that include a servo gun axis (from real robot or from your Kuka contact)
08-12-2015 11:45 AM
I tryed to put the Machine.dat file from a backup, into a folder MachineDataFiles in the systroot.
Two machine.dat, one inside the KRC/Steu/Mada and another inside of KRC /R1/Mada.
But now the RCS doesnt start because erro -56, machine data not found.
08-12-2015 11:48 AM
You should not do this manually, instead you should use Robot Setup / Load Machine Data facility.
08-12-2015 01:03 PM
I did it in both ways.. First of all put manually, and after by Load Machine Data. And it did´t work..
another ideia?
08-13-2015 09:41 AM
I compared the machine.dat of robot backup with KRC4 file from KukaFtp, and tryed to see where the line that generates a error of dat file not founded. The line is:
INT $EX_AX_NUM=0 ;ANZAHL EXTERNER ACHSEN (0-6)
If I put 1 in the axis number, the rcs give me a error.
Must I do a external axis configuration before load a dat file?
08-17-2015 04:27 AM - edited 08-17-2015 04:28 AM
Some backups were missing files needed by the RCS. For instance E1.xml from Config\User\Common\Mada\NGAxis was sometimes missing...
02-16-2017 09:39 AM
Hi, I have a similar problem.
Where i can get the correct RRS files for Track robots and Servo guns
Thanks
02-18-2017 04:34 PM
For Kuka robots you should use tools like SyncroMove or Work Visual to configure Servo guns as external axis.
For Tracks you have to use the machine datas in the external axis folder (e.g. KL1500)
02-18-2017 06:12 PM
Thanks for the information
Now where can I download the Mada file for KL1500, I look all Siemens pages and I could found.
Normally the robot is mounted on it is KR420_3330.
Thanks for any help
Watch Replays of Previous Topics