Showing results for 
Search instead for 
Did you mean: 

Kuka RCS


I have downloaded Kuka RCS:


rcs_kuka_MKS_krc5.6_r02.00_21.09.2010.MKS91_PC and Mada-Krc5.6_r02-V3.8.1-KRC2.


Do I also need the MKS Toolkit Application? Which is the correct one for this version of the software and is it on GTAC?


Re: Kuka RCS

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, this version requires MKS runtime. The correct MKS version is 9.1 or above. It is automatically installed when you install Robcad. It is not included in Process Simulate, nor it is available independently on GTAC.

Re: Kuka RCS

OK thanks. I am using Process Simulate 10.1, how can I acquire MKS Runtime?


Paul Hogan
Cosma Assembly Technology (CAT)
905 799-7600 x5419

Re: Kuka RCS

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

If possible download Robcad, which includes the MKS ToolKit.

If not, contact hotline of Siemens PLM via GTAC and they can give it to you.

These are the official ways.