Cancel
Showing results for 
Search instead for 
Did you mean: 

License error for ABB RCS 6.01

Experimenter
Experimenter

Hello,

 

I have been using ABB RCS 5.xx for a long time now.

We recently changed over to RCS 6.01. When I am trying to run a robot using this RCS, I get the following error;

 

Errors:

1)    IRB6700_200-280_SW_IRC5_Grey[RRS]> Note at (Weld_Op) via: RRS Message: ERROR:

2)                                                              50290: Service unavailable

3)                                                              Unable to obtain correct license.

4)                                                              

5)                                                              Please check the license settings.

6)   IRB6700_200-280_SW_IRC5_Grey[RRS]> Error at (Weld_Op) via: Motion Failed: Internal software error., Error Code: -49

 

 

Is there a special license for ABB RCS 6.xx?

 

Best regards,

Henrik

1 REPLY

Re: License error for ABB RCS 6.01

Siemens Phenom Siemens Phenom
Siemens Phenom

yes, you need another licence for RW6 (different from the one used for RW5). Note that you can use the same RCS server for both.