06-08-2015 09:11 AM
Dear creative experts,
because some people are asking for capturing movies, I believe they are not aware of the download-section. There is an entry named "High Quality Movie Capturing".
I'm taking the opportunity to move my project over to this thread now, pls ignore the other download location from now.
Movie Capturing
Attached MovieCapture-package includes:
Comments, Kudo's, created movies and anything that pushes my motivation to continue the project is highly appreciated ;-)
06-10-2015 11:17 AM
Hi Guido!
I want to try MovieCapture and RealTimeSync, but I have some problems to add the buttons to a toolbar.
I copied the DLLs to the DotNetCommands-Folder and the XMLs to DotNetExternalApplications.
Then I started PS 11.1 on Win7 x64.
But there is no AddOn category and there are no commands for MovieCapture and RealTimeSync in the All commands category - see picture.
06-10-2015 11:33 AM
that sounds bad...
It should definitly work on 11.1 without problems...this is really strange.
Please double check, that the path is like eMPower\DotNetCommands\MovieCapture.dll
If correct, let's try to recreate the xml's.
If that doesn't work, I need to check.
06-10-2015 11:40 AM
Hi Guido,
I tried this already.
The following error always occur.
06-10-2015 12:19 PM - edited 06-10-2015 12:21 PM
This is a win 7 problem...
The dll is locked by windows itself.
Solution: right-click on the dll. In the properties (general tab) you will find "unlock" in the bottom right corner
06-10-2015 01:22 PM
06-10-2015 01:36 PM
Yes, this is an automatic safety mechanism if you obtain your dll directly from internet.
Win 7 locks the dlls to prevent from automatic execution.
06-11-2015 01:46 AM
Good morning!
It works now! Thank you Patrick for the hint.
Maybe the package should be provided with an installer.
06-11-2015 05:20 AM
Hello GuidoDamm,
Thank you for this amazing Moviecapture feature. I tried it roughly a month ago and it worked like a charm!
Tested it with PS version 12.0 on Win7.
Best regards
SaMe
06-11-2015 06:05 AM
Watch Replays of Previous Topics