Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple part appearances in OPC-simulation

Pioneer
Pioneer

Hello,

Is there any way to end all the appearances of one part at the same time?

I tried it with Non-Sim operation and noticed that, for example, if there is 5 appearances of part1, I have to click "end_material_flow" -key signal for five times to make all the appearances disappear.

 

Best regards

SaMe

2 REPLIES 2

Re: Multiple part appearances in OPC-simulation

Genius
Genius

Hi

 

just out of curiosity, what is the reason behind wanting to end all the appearances at the same time?

 

BR

Andreas

Re: Multiple part appearances in OPC-simulation

Pioneer
Pioneer

Hello,

 

There is an assemby which my robot assembles where I use 5 appearances of one part and after it is ready I want those 5 appearances to vanish and at the same time one appearance of the whole assembly appear. So it would be easier to handle just one appearance rather than 5 since it is not possible to use Attach Object in OPC-simulation?

I know I could use Substitute Instances to compound these appearances into one but I don't know how to use it and at the moment I don't have time for that.

 

Best regards

SaMe