cancel
Showing results for 
Search instead for 
Did you mean: 

NO pathtemplateconfiguration folder in default folder

Experimenter
Experimenter

Hi All,

I am a very newby here!!!

I have multiple questions:

I've downloaded robotexpert 13.0.

I have been trying to follow the youtube videos for beginners and  I am stuck at RobotExpert5 - OLP (Chapter A) because of  the following reasons:

1) the menu bar is different in version 13.0 ( the video has  a version 12.0) and thus I do not find the 'Apply Path Template Action' under 'Path Editing' in the 'Operations' tab.

However, 

2) I find a button called 'Apply Path Template' Which I reckon this is where I should edit path.

When I click on it I got a message such as

       'Some problems were encountered in the XML(s).

        Open Customized Commands XML Checker?'

When I click 'Yes', a window pops up where I get warnings after each path:

 

 

'DataConfiguration:
Path:
C:\Program Files\Tecnomatix_13.0\eMPower\Robotics\OLP\default\DataConfiguration

Warning:
This folder is missing for controller: "default".

OlpConfiguration:
Path:
C:\Program Files\Tecnomatix_13.0\eMPower\Robotics\OLP\default\OlpConfiguration

Warning:
This folder is missing for controller: "default".

MotionConfiguration:
Path:
C:\Program Files\Tecnomatix_13.0\eMPower\Robotics\OLP\default\MotionConfiguration

Warning:
This folder is missing for controller: "default".

PathTemplateConfiguration:
Path:
C:\Program Files\Tecnomatix_13.0\eMPower\Robotics\OLP\default\PathTemplateConfiguration

Warning:
This folder is missing for controller: "default".

DownloadTemplatesConfiguration:
Path:
C:\Program Files\Tecnomatix_13.0\eMPower\Robotics\OLP\default\DownloadTemplatesConfiguration

Warning:
This folder is missing for controller: "default".'

 

Can you please, tell me what is this contoller I am missing and where to find it to download and how to implement in my software to be able to finish the video tasks ?

Thank you !

 

 

2 REPLIES

Re: NO pathtemplateconfiguration folder in default folder

Siemens Experimenter Siemens Experimenter
Siemens Experimenter
Hi, It sounds like an issue so I'll check it further with R&D. In any case, in order to avoid it, you can create your own these folders. Please browse to : "C:\Program Files\Tecnomatix_13.0\eMPower\Robotics\OLP\default" and create 3 new folders: "OlpConfiguration", "MotionConfiguration" and "PathTemplateConfiguration". This should be enough at this point in order to complete the video guide tutorial. Regards Sefi

Re: NO pathtemplateconfiguration folder in default folder

Experimenter
Experimenter

Thank you Sefi!

It did work and was a very simple solution.

Regards

G.O.