Cancel
Showing results for 
Search instead for 
Did you mean: 

OLP Command doesnt read a robot signal - CEE

Pioneer
Pioneer

Hello Everybody,

 

I am having a problem with a OLP Command in a CEE Simulation. (PS 11.1)

 

I ve creaded 2 signals into Robot Signals. ("selectSx", "selectDx")

 

 

 

I am trying put a IF OLP Command into a Main program. I put in the right way and the simulation doesent go ahead, and when I push pause give me a error "Signals are currently ignored".  (I've tested in another PC and it works), 

 

#If selectSx AND NOT selectDx then
# CallPath Prelievo_staffa_sx_226
# CallPath Spalmatura_sx_226
# CallPath Deposito_staffa_sx_226
# CallPath Weld_Op10_226_sx
#EndIf
#If selectDx AND NOT selectSx then
# CallPath Prelievo_staffa_226_dx
# CallPath Spalmatura_226_dx
# CallPath Deposito_staffa_226_dx
# CallPath Weld_Op10_226_dx
#EndIf

 

 

Must I have another configuration?

 

Thanks

2 REPLIES

Re: OLP Command doesnt read a robot signal - CEE

Siemens Phenom Siemens Phenom
Siemens Phenom

For the signals to be active you need:

1) to be in Line Simulation Mode

2) to simulate the Line Operation (root node)

3) to make sure signals are not explicitly ignored (in Tools / Options / Motion, there is a "Ignore Signals" option)

Re: OLP Command doesnt read a robot signal - CEE

Pioneer
Pioneer

Solved,

 

I ve just found it on Options>Motion.

 

Thanks Gilles Velay I found it few minutes  before you anwser, but thanks for atention.