Cancel
Showing results for 
Search instead for 
Did you mean: 

OLP command with mutiple layer

Experimenter
Experimenter

Hi all, I need to create OLP command to insert name of welding point, after welding point name is inserted I want to cliick on it and dialog with this name should pop-up where I can change the name. Is it possible?

4 REPLIES
Highlighted

Re: OLP command with mutiple layer

Experimenter
Experimenter

I need to use item dynamic parameter as a Default value

<Param Name="Comment" UseLocationParamVal ="true" Default="Loc Name">

<Item Type="dynamicParameter">Loc Name</Item>

Re: OLP command with mutiple layer

Siemens Phenom Siemens Phenom
Siemens Phenom

I would suggest a XML Path Template to populate your regular parameter with dynamic parameter "Loc Name" then you would edit your regular parameter.

 

There is no way to defined default value for a regular parameter based on a dynamic parameter.

Re: OLP command with mutiple layer

Experimenter
Experimenter

Can you show me the example of action which do that? And how do I use this parameters as default value? Thanks for answer

Re: OLP command with mutiple layer

Phenom
Phenom

Hello ElSombrante

 

Can you explain a little more about your need?

 

You can also populate MFG names automatically using "RoboticParametersToMfgAttributes.xml" located under your SystemRoot directory.

 

In addition to that, you can edit the Name in a specific motion parameter and use this parameter in Path Editor (so you don't need to open an OLP command each time).

 

But all of this depends on your needs